6/10/2015 2:14 AM | |
Posts: 1 Rating: (0) |
hi Do we need to do reconfiguration or change any other thing when the simatic S7, digital input SM326 SM32624DE, 24V, fal. save part No. 6ES7326-1BK01-0AB0 is replaced by 6ES7326-1BK02-0AB0? Same question for simatic S7, digital output SM326 , part No. 6ES7326-2BF40-0AB0 when is replaced by 6ES7326-2BF41-0AB0. BR
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/11/2015 9:21:18 AMNew subject after splitting |
|
6/11/2015 8:47 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
they are both spare part compatible, like you can see in the following entries: |
FCK WAR! |
|
6/17/2015 4:49 PM | |
Posts: 366 Rating: (30) |
Ok I'm sorry for the wrong information.. Thanks! nice regards |
3/21/2016 9:29 AM | |
Joined: 3/2/2007 Last visit: 4/26/2024 Posts: 929 Rating: (5) |
thank you for all the valuable information... |
... thank you ... |
|
Follow us on