7/5/2021 9:46 AM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating: (380)
|
Hi, the IndOS is pre-installed on your device. The very first indicator for this is the STAT LED being off, when no SD card / USB is plugged. If the IndOS wouldn't be installed, the STAT LED would be red in this case. When there is no monitor available the only option is to use a UART cable (e.g this) and establish a serial connection via putty. You can then either configure the IndOS or change the boot order to boot from SD card with Example Image. You can "recover" your SD cards with Windows 10 with the following steps:
Now the card is empty again and can be detected with Windows Explorer. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
7/5/2021 10:10 AM | |
Joined: 1/27/2020 Last visit: 1/14/2025 Posts: 2 Rating: (0) |
Thank you bergmanu! |
Last edited by: AutoGen_2098290 at: 07/05/2021 10:10:36 |
|
Follow us on