2/7/2024 11:01 AM | |
Joined: 5/6/2022 Last visit: 6/21/2024 Posts: 424 Rating: (83) |
Hi PetrNowak, From what I have been able to find, I think that the Backup takes the OS Image as well but it seems that if you do it with the memory card as you can see in point 2. With Prosave it does not seem to indicate anything. Although it is true that it is not entirely clear whether he takes it or not. Here is the link to the FAQ: "How do you backup/restore with a Windows-based panel?" If I find something new I'll let you know! Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on