8/10/2021 8:44 PM | |
Joined: 8/6/2021 Last visit: 3/25/2022 Posts: 2 Rating: (0) |
Since it has been 3 years since this question was raised I would like to revisit it. The LOGO has an ethernet connection and we are able to upload and download programs. It is intuitive that email capability would be build in without the need for additional hardware. I would like to send email and/or sms messages when a certain condition occurs. Does the current version of LOGO! plc have the ability to sent email and/or sms messages? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/11/2021 10:58:32New subject after splitting |
|
8/11/2021 9:52 PM | |
Joined: 12/18/2014 Last visit: 9/16/2024 Posts: 33779 Rating: (4194)
|
Or some like this: |
8/12/2021 7:21 AM | |
Joined: 9/11/2014 Last visit: 9/16/2024 Posts: 750 Rating: (29) |
Hi, here an example how it is possible by using LOGO! and AWS cloud: https://support.industry.siemens.com/cs/de/de/view/109799625 Sorry this I only found in German. |
Follow us on