5/3/2018 6:01 PM | |
Posts: 1 Rating: (0) |
hello , I don't have CPU 416-5H in HW CONFIG even I have installed the update materiels . What can i do appear it in the interface ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/4/2018 7:34:16 AMNew subject after splitting |
|
5/4/2018 7:35 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hello, which Software you use and which version? Christoph |
5/4/2018 11:57 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928)
|
Hi stormatchou, When you open the hardware configuration, you can see on the right top side (default position) the catalog you are using. It is listed under: "profile". Normally in PCS7, the PCS7 catalog is selected-> "PCS7_V90" for example. This means only modules, CPU's and other are visible which are released for your current PCS7 version. What happens if you select the "Standard" catalog? Is the CPU selectable? If so, the CPU you are using is not released for use with PCS7 (at least the version you are using). What also can be the case is that you have a newer CPU, in order to use it, you need to configure an older version CPU so you are basically operating the newer CPU with older CPU firmware. It may be that you won't get to use new functionalities.... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on