Industry Online Support
Technical Forum
7/30/2008 5:44 PM | |
Posts: 2661 Rating: (279) |
Hi, In the attachment I do not see Q0.0 or Q99.0! But I do see the formal operands or function block parameters of type "Q" in FB31. These Q's represent the parameter type OUTPUT and are different from digital output also represented by "Q". Confusing, ain't it?So when you call the FB31 in another block, you can pass-on a "Q", "I" or an "F". I think you should begin reading the S5 manuals! See links bellow: S5-135U CPU 928B Programming Guide S5 Manuals for Download Regards |
Last edited by: Phantom75 at: 7/30/2008 7:51 PM |
|
Follow us on