2/1/2014 4:20 PM | |
Posts: 5 Rating: (0) |
My question is simple : Is the PC-ADAPTER USB (MPI/DP) can be used to transfer the vue from Wincc flexible to a KTP600 COLOR DP. |
2/1/2014 10:45 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello zidznoi; Yes, you can use the USB-PC Adapter cable to download and upload to a KTP600 basic color DP panel. See the table in the following FAQ for details: Which connector cables are available for connecting to SIMATIC Panels? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/1/2014 10:46 PM |
|
3/13/2014 11:04 PM | |
Posts: 5 Rating: (0) |
I tried several time to do the transfert to the KTP600 DP Color via a PC adapter USB from a PC (winccFlexible) but no result. What's to do ? |
Follow us on