9/14/2016 11:06 AM | |
Posts: 3609 Rating:
|
Import of a technical question from the user Mayur.K
|
9/14/2016 2:30 PM | |
Joined: 7/7/2010 Last visit: 4/28/2025 Posts: 15823 Rating:
|
I have to wonder if the PLC is the correct model if it works on the 1215. Maybe you have the 1215 in the project copied to the MMC? Try simply downloading the project to the PLC. If it refuses, you have the wrong PLC in the project.
|
science guy |
|
This contribution was helpful to
1 thankful Users |
Follow us on