1/15/2013 6:36 AM | |
Joined: 3/15/2011 Last visit: 1/7/2025 Posts: 134 Rating:
|
Dear All, Fault code 1044 and 1043 are coming when a download is carried on G120 Drive with CU-240E-2 FIRMWARE VERSION 4.5. Please note that I ‘m using a current Starter Version 4.3.1.2 which is the latest one. I have attached a Snapshot of the Project .Please suggest a solution for this
AttachmentERROR_MESSAGE123.pdf (496 Downloads) |
1/24/2013 10:13 AM | |
Joined: 3/15/2011 Last visit: 1/7/2025 Posts: 134 Rating:
|
Please note that i have tried these two projects in two different CU.But faced the same problem.I'm attaching the Project.Hope you get some clue
Attachment12_01_2013_FD_FAN.zip (303 Downloads) |
1/24/2013 1:50 PM | |
Joined: 3/15/2011 Last visit: 1/7/2025 Posts: 134 Rating:
|
Hi, The Firmware of the CUis 4.5.what else do i need to update.Please Clarify Regards Ashutosh Kr Verma
|
1/25/2013 5:39 AM | |
Joined: 3/15/2011 Last visit: 1/7/2025 Posts: 134 Rating:
|
Hi ChristophD please note that i 'm not using any MMC card.The data is laoded in the CU itself. Regards Ashutosh Kr Verma
|
Follow us on