7/17/2009 12:42 AM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating: (20) |
Hi there. Good luck. |
Keep working! |
|
7/17/2009 9:57 AM | |
Posts: 163 Rating: (0) |
I get the following error.I feel there is some problem in the downloading cable.CPU412-3H controller has one port MPI/PROFIBUS which can be configured as either of one. Attachment1 Hardware Download error.zip (180 Downloads) |
7/17/2009 11:46 AM | |
Posts: 325 Rating: (13) |
Hi Sindhu, Even I used to get kind og messages and basically the problem is with Set PG-PC interface. I suggest u have a look at the same. Regards Nil |
7/17/2009 12:23 PM | |
Posts: 163 Rating: (0) |
What is meant by SDB receiver,the error shows the SDB receiver may be in wrong mode |
7/20/2009 8:24 AM | |
Posts: 163 Rating: (0) |
Yes its PC Adapter MPI Cable (USB-MPI).But the local support says that it will support Profibus also?is that right? |
Follow us on