9/27/2018 5:03 AM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating: (4148) |
There's no attached photo. |
9/27/2018 1:41 PM | |
Joined: 2/10/2016 Last visit: 6/13/2024 Posts: 115 Rating: (0) |
sorry I have updated the post with the attachement |
9/27/2018 5:19 PM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating: (213) |
Hello, 1-Perhaps the attached file might help. Windows Device Manager Ports(COM) Communication Port(COM1) Port Settings Advanced Set the "Buffer"to a low value. 2-Transfer mode in OP7: Press and hold the keys 'ESC' and 'Cursor Up' while turning on the power supply of the panel. |
Eng.Mohamed Ibrahim |
|
9/29/2018 12:23 PM | |
Joined: 9/21/2012 Last visit: 7/26/2024 Posts: 4037 Rating: (455) |
What other options does the COM list give? You should look from Device Manager to see what COM ports are active. |
Follow us on