5/20/2012 12:26 AM | |
Posts: 2661 Rating: (279)
|
There could be many reasons. Can you describe your bus structure (Plant Bus/Terminal Bus)? Which messages may appear in the "Download OS" dialog box? How do you use the SIMATIC shell to configure the terminal bus of a WinCC station? |
This contribution was helpful to1 thankful Users |
5/20/2012 12:41 AM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Hello again! I guess you will understand the problem after reading my answer to your previous question. You should not share a hole partition, but just a folder. And it's name should differ from the WinCC Application name. And before downloading to the OS Station, please, try at least run the cmd command "ping <computername>" to be shure that "RT Station is obtainable". I doubt that you have renamed the target PC ESOS1 to OS, or I am wrong? |
5/20/2012 1:01 AM | |
Posts: 95 Rating: (0) |
Thanks, I got that solved. In fact, I shared a folder 'OS', and it doesn't like the path \\ESOS1\OS\OS.mcp, and I entered \\OS\OS.mcp and it passed. Wierd?! But I did use this way to fulfill the OS downloading before - just I don't remeber the details. Now the question is I cannot download OS - Which worked
|
Follow us on