9/22/2016 10:16 PM | |
Joined: 7/20/2016 Last visit: 5/20/2024 Posts: 3 Rating: (1) |
I downloaded the file and unzipped it. Ran as an administrator and it starts to run but it stalls while in the cmd prompt and just sits there doing nothing. I noticed that the file is only 1kb. Should it be that small? Any help would be appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/23/2016 1:59:38 PMNew subject after splitting |
|
9/23/2016 5:27 AM | |
Joined: 12/18/2014 Last visit: 10/9/2024 Posts: 33922 Rating: (4216) |
Then, the download is not complete. Start the download again. The download file has a size of 684 MB. |
9/23/2016 2:29 PM | |
Joined: 7/20/2016 Last visit: 5/20/2024 Posts: 3 Rating: (1) |
Ok thanks. Is this the link to the PCP/PPI cable patch update? Im getting access point not found when trying to connect. |
Follow us on