6/4/2011 4:01 PM | |
Posts: 204 Rating: (1) |
Hi, I try now to download my prog. but it's fail... when I power on the OP27, I Can't entered the download mode....I don't know why??? I clik up+esc no action.... my OP27 is new What I should do? I didn't found 9pin to15 pin converter, I must built it because I read that in manula" i must program through IF2 ", I need the pins diagram.. Thanks splitted from protool need. |
Last edited by: O_Moderator at: 6/7/2011 9:37 AMnew subject after splitting |
|
6/4/2011 4:28 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Try it: 1. Power supply is OFF. 2. Press ESC+ ArrowUP and keep 3. Power supply is ON. 4. Release the buttons. Pin layout of serial cable (6XV1 440-2KH..) http://support.automation.siemens.com/WW/view/en/29034071 best regards, Hristo Mihalev |
6/5/2011 2:02 PM | |
Posts: 204 Rating: (1) |
Thanks ayman are I must be connected with PC when tring that |
6/5/2011 8:12 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Please contact with Support Request. Best regards, Hristo Mihalev |
Follow us on