6/25/2016 12:19 AM | |
Posts: 3 Rating: (0) |
I am having problems downloading the data from my ES to my OS. The error that I am getting is the following: Error coping the project data to the destination system. I followed the path and the file destination is a OSAS.ldf. However, the file on the destination have a diferent file termination OSAS.mcp. I change the path to the OSAS.mpc and I have the same problem again. So Far, I can't download new graphics on the WinCC Runtime. From my SIMANTEC MANAGER Please advice. Thanks, Rolando AttachmentCopy of ERROR download.pdf (337 Downloads) |
7/17/2016 4:54 PM | |
Joined: 7/10/2012 Last visit: 9/26/2024 Posts: 1 Rating: (0) |
I am having the same problem, some expert could help? |
Follow us on