10/2/2017 10:44 AM | |
Posts: 51 Rating: (0) |
Hello, Can I download and use scout v4.1 and 4.2 at the same time in one PG. Thank you. |
10/2/2017 10:47 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hello, no this is not possible. But why you would do this? Regards Christoph |
10/2/2017 1:10 PM | |
Posts: 51 Rating: (0) |
Because I dont want to convert to program 4.1 to 4.2 because the others make a remote connect to machine with v4.1 and they cant open it. |
10/2/2017 1:15 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hello, you can use the Option Save in older version, so the project can be opened in V4.1 again.
Christoph |
10/2/2017 1:43 PM | |
Posts: 51 Rating: (0) |
Hello, For example If I download v4.2 to d445, the remote connecttor cant connect with v4.1. |
10/2/2017 3:29 PM | |
Posts: 51 Rating: (0) |
You said, I change something in new version and then If I save it as an old project format and download it, It will be old version in d435. King regardsç |
Follow us on