8/5/2016 5:10 PM | |
Posts: 35 Rating: (0) |
I too am having problems downloading to a KTP700 Basic DP. I have an S7-200 which I am having to program with Microwin and the KTP700 which I have written the program with TIA Portal V13 sp1. The software is completely up to date, but when I come to download, it only gives me the option for Teleservice, nothing else. This is the first time I have used Portal so you will have to excuse my shortcomings. I have checked the means of download in the project tree and that says ok. Any help would be very appreciated. Rob ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 8/7/2016 10:38:02 AMNew subject after splitting |
|
8/8/2016 9:55 AM | |
Posts: 35 Rating: (0) |
Hi again, Can I just email you the project? I think I am missing something, settings or missing info. Regards Rob |
8/8/2016 11:17 AM | |
Posts: 35 Rating: (0) |
OK Christoph, I have done as you said. The image is attached. Regards, Rob |
Follow us on