Industry Online Support
Technical Forum
12/2/2009 9:30 AM | |
Joined: 4/24/2006 Last visit: 5/2/2024 Posts: 8629 Rating: (1147) |
Dear annupalani, In both SIEMENS PLC's you need to include the DP/DP coupler in HW configuration. It is a DP slave with an unique profibus address. It can be different DP slave address on both HW-configurations. Then you will have to configure the amount of Bytes you want to communicate between the PLC's Here is a link to manual: DP/DP coupler Best regards, Wizard |
Last edited by: Wizard at: 12/2/2009 9:32 AM |
|
Follow us on