3/27/2019 1:59 PM | |
Joined: 5/30/2017 Last visit: 9/8/2023 Posts: 3 Rating:
|
Hello HAti, I would like to thank you for showing interest in this problem. This is my situation, I have set same address in HW config and DIP as 3. ADDR=OFF, DIA=OFF, PS=ON and all rest are OFF. DP-DP coupler installed is V3.0.1 and so i downloaded GSD for DP_DP Release 3 from this Link01 Pls correct me if i have to use DP-DP release 2 in HW Config. Find the attached pic of my hw config as well as my diagnostic buffer in a single pic and help me solve this out. Thanks in advance Regards, Devanand J |
Follow us on