10/24/2008 4:56 PM | |
Posts: 1 Rating: (0) |
Hi, I have a problem withDP DP couplers that don't reconnect after a PB linebreak. Please see the system on attached schematic. When I test redundancy, by pulling the line from AC800Mon DP DP A and insert it back, all LED's are on (SF2, BF2 flashing, rest is steady). It stays like this, until I: 1: pull the line into network 1 on DP DP B, then a redundancy switch is made and DP DP A reconnects. But then DP DP B is not reconnected. 2: pull/reinsert or turns off end resistor on network 2 on DP DP A. All seems thennormal. If I pull/reinsert line from AC870P (network 2), it reconnects without a problem. Observations: Pulling network 1 lines: SF1 and BF1 is steady on. Pulling network 2 lines: SF1, SF2 and BF2 is steady on. When I have this flashing as described above, it seems like the network 2 is on and off. Tracing the line shows a couple data exchanges before it's down again. Thanks Torbjørn Skjeggestad AttachmentDP DP network.pdf (171 Downloads) |
Follow us on