7/4/2013 8:29 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi JoeGrib, and do not forget that the number of BYTE for the exchange between the two masters must be the same. |
7/4/2013 8:45 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
OFT I would transfer the data in DINT instead of REAL.
|
7/4/2013 8:52 AM | |
Joined: 9/16/2011 Last visit: 6/20/2024 Posts: 291 Rating: (6) |
DearUMENCHO, Why DINT, not REAL ? both will occupy 4 bytes...........
|
Reg, |
|
7/4/2013 9:11 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello UMENCHO, Have a look: DP/DP Coupler The data is sent in BYTE, so there is no problem. |
7/4/2013 2:42 PM | |
Posts: 6 Rating: (0) |
word type has 2 bytes length? |
7/4/2013 2:47 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi J86Obalhe, 8 BIT -> 1 BYTE 1 WORD -> 2 BYTE 1 DWORD -> 4 BYTE 1 REAL -> 4 BYTE |
Follow us on