4/13/2010 8:48 AM | |
Posts: 12 Rating:
|
Hello Users! I´m beginner in Siemens and I have a simple question. Which is the difference between DP_SEND and DPWR_DAT blocks ?When each one is used ? Thanks |
4/13/2010 12:18 PM | |
Joined: 8/25/2005 Last visit: 6/12/2024 Posts: 1162 Rating:
|
Hello Licht, The DP_Send is only used in combination with a CP342-5. The DPWR_DAT is necessary to transfer consistand data to a module with 3 or more as 5 Byte data. Have a look at the following manuals for details: S7-CPs for PROFIBUS Configuring and Commissioning Automation System S7-400 CPU Specifications Best regards Sabine |
4/14/2010 3:39 AM | |
Posts: 12 Rating:
|
Hello Sabine, Thank you for the links. But I still have a question: Can I use DPWR_DAT instead DP_SEND block whether I amusing a CP342-5 ? Thanks ! |
Last edited by: Licht at: 4/14/2010 3:40 AM |
|
4/14/2010 6:15 AM | |
Joined: 10/7/2005 Last visit: 6/28/2024 Posts: 3008 Rating:
|
Hello Licht No you can NOT, you MUST use DP_SEND for a CP342-5 and below are a couple of FAQ's which have moreuseful info on this subject: What are the differences between an integrated DP interface of my CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5? What should you watch out for when configuring a CP342-5 as DP master? I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on