5/4/2020 6:05 PM | |
Joined: 1/9/2017 Last visit: 11/9/2023 Posts: 13 Rating: (0) |
Good day. In the "Old Project" configuration: CPU 315-2 DP 6AG1 315-2AG10-0AB0 V2.0 + 6SL3040-0xA00-0xxx Firmware ???? . I am creating a new project "New" with the same devices and not get the same configuration. If you add "SINAMICS" to the project, then "DP Slawe" is not displayed in "Hardware", so there is no way to configure telegrams and addresses. When SINAMICS is added to Hardware, the devices are added to the SIMATIC 300 folder, but other tabs in the Object Properties. What needs to be done to get similar to the "Old Project". I hope for your help.
AttachmentSaved Pictures2.zip (33 Downloads) |
5/4/2020 6:55 PM | |
Joined: 1/9/2017 Last visit: 11/9/2023 Posts: 13 Rating: (0) |
I can not find the GSD file. The forum has a few posts about this file, but there are no links. |
5/4/2020 6:59 PM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979)
|
hello, check it here |
This contribution was helpful to1 thankful Users |
Follow us on