8/19/2019 7:39 PM | |
Joined: 12/25/2018 Last visit: 4/24/2024 Posts: 76 Rating: (0) |
module |
8/19/2019 8:23 PM | |
Posts: 7 Rating: (0) |
Try to replace those Power Unit modules. |
8/19/2019 10:41 PM | |
Posts: 7 Rating: (0) |
Are the Power units the same model and version? Since they are, you can do it. |
8/19/2019 11:10 PM | |
Joined: 12/25/2018 Last visit: 4/24/2024 Posts: 76 Rating: (0) |
they are same machines of same manufacturer. i just want to confirm that the module get damaged not because of motor. |
8/19/2019 11:21 PM | |
Posts: 7 Rating: (0) |
You said you've checked the motors and they're good. It doesn't seem the problem are the Motors, In this case. It seems The modules are the problem. |
Follow us on