8/18/2016 4:31 PM | |
Joined: 5/16/2016 Last visit: 5/21/2024 Posts: 42 Rating: (7) |
First I suggest you get the compendium from here https://cache.industry.siemens.com/dl/files/407/13472407/att_88465/v1/mc24_kompend_e.pdf You can reference the control word bits on pages 934 to 935, diagram 180 and 190. Also, do you have the profibus daughterboard installed? Refer to diagram 120 in the manual, page 917, to determine the addresses you need to write for the control word. Start from here, you if need more help just post it and I will reply. |
Why you troubleshoot? |
|
Follow us on