9/10/2019 11:00 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
Do I understand correctly that if I want to make a cable similar 6FX2002-1DC00-1BA0 (10m)? I need to order: #1 6FX2003-0DC20 (2 pcs.) - SIGNAL CONNECTOR, RJ45 IP20 #2 6FX2008-1DC00-6FX2008-1DC00-1BA0 Signal cable sold by the meter type: 6FX2008-1DC00 (DRIVE-CLiQ) 2x2X0.22 C not trailable (10m) #3 82-00061 (yamaichi.de) (1 pcs.) – Crimping tool HT-2008R-Plus-1.0 (Crimping tool for RJ45/IP67 and RJ45/IP20) ---------------------------- How can I understand in which case I need cable with 24 V or without 24 V? is there any list in which cases is necessary or not 24V? Eg. cable between CU320 – 2 PN and SLM (SMART LINE MODULE)? Sizer configures this cable as 6FX2002-1DC00-1BA0 (without 24 V)! Instead DRIVE CLiQ cable (without 24 V) Can I use standard ethernet patch cord eg. 6XV1870-3QH20? |
Last edited by: _oleksandr_ at: 09/10/2019 12:18:51Last edited by: _oleksandr_ at: 09/10/2019 12:19:54 |
|
6/22/2022 9:45 PM |
|
Joined: 9/29/2017 Last visit: 5/14/2024 Posts: 1 Rating:
|
The point is Siemens delivery issues can be extreme on Drive Cliq cables. |
Follow us on