10/15/2009 9:27 AM | |
Joined: 4/24/2006 Last visit: 9/12/2024 Posts: 8736 Rating: (1167) |
Dear isurya, Normally the Driver is installed, when installing Step 7 Microwin. Look at PG/PC interface, here you find PC/PPI cable, go to properties and tab Local connection. (Here it should be possible to choose USB) Here you can download SP7 for Step 7/MicroWin v4.0: http://support.automation.siemens.com/WW/view/en/33005232 Best regards, Wizard |
2/2/2016 10:09 PM | |
Posts: 20 Rating: (0) |
can you help me please to download the driver? |
2/3/2016 7:12 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
Hello, there is no download for the drivers available, the drivers integrated in Step7 MicroWin. Regards Christoph |
2/3/2016 7:34 PM | |
Posts: 20 Rating: (0) |
thank you |
2/21/2017 4:47 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by mei2010 is split to a separate thread with the subject How can i setup Microwin without the previous version?. Best regards |
Follow us on