12/6/2021 8:43 AM | |
Joined: 1/11/2019 Last visit: 7/1/2024 Posts: 727 Rating: (144) |
Hi, The protection of SIMIT basic components from e.g. the Drives are protected by passwords and those passwords are not available. If you are interested in SIMIT component creation with CTE, Siemens recommend the SIMIT manual, and these two below links are of SIOS application examples. Creating a SIMIT component with CTE SIMIT CTE - Creating a component in one hour Hope it helps you! |
Follow us on