4/19/2016 9:29 AM | |
Joined: 11/21/2007 Last visit: 12/23/2024 Posts: 2325 Rating:
|
Hello Pl answer the questions of PISCEAN 2010 In addition, pl check if the Address of your PC Adaptor is not same as assigned to any of the nodes on the network. Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
4/19/2016 9:51 AM | |
Joined: 8/25/2014 Last visit: 10/3/2024 Posts: 166 Rating:
|
Dear Experts, I am explaining more. I have 5 nodes and parker 890ssd Drives as well. These 5 nodes have CPU's. All are same type of CPU's (CPU 315-2 PN/DP). PISCEAN 2010Dear Piscean:- I connect the the PD thorugh profibus connector and it is not communicating and the Cpu goes to SF/Bf and alarm appears on the PG (Connection lost). But when I removed the profibus connector and cable from CPU and directly connect the PG wth the CPU it is communicating. While showing error thorugh profibus connector I couldn't go online that's why I cannot check in the buffer of CPU. But the error shows for 1 sec. Arasanprofibus address is correct one. The machine is running there is no problem with the machine but my issue while I try to communicate with the PG, this happens. NavnagI check the PC adaptor address. it is not conflict with the address of others. |
4/19/2016 9:54 AM | |
Joined: 8/14/2014 Last visit: 4/5/2024 Posts: 144 Rating:
|
Have you checked if any connector hasn't loosen inside? I mean unscrew them and check cables connection |
4/19/2016 10:09 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Ok. Please check the terminator resistor position at that profibus connector. Is it OFF or ON? |
Follow us on