10/29/2024 7:51 AM | |
Joined: 1/21/2013 Last visit: 3/14/2025 Posts: 3650 Rating:
|
Hi, The Graphics View element can only display graphics that are included in the compiled project. The Web Control object can access files in the home folder or on an external storage device. However, the performance of the Web Control is inferior to that of the Graphics View. And the Web Control on the UCP cannot access external files when accessing the Runtime via the Web Client. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on