10/2/2024 2:45 PM | |
Joined: 2/26/2024 Last visit: 10/5/2024 Posts: 48 Rating: (0) |
Hi, How can the attached dynamic svg animated (in rotation) when running the HMI program? |
10/3/2024 1:35 PM | |
Joined: 11/13/2018 Last visit: 10/3/2024 Posts: 32 Rating: (4) |
Hello AutoGen_8472461, You don't need to search for the element or set an attribute You need to write a value between 0 and 360 in the variable ‘value’. You can vary that value based on the time. The trigger (clock icon) allows you to choose when the script should be executed (e.g. every 100ms). I recommend taking a look at: Tips and Tricks for Scripting |
10/3/2024 1:50 PM | |
Joined: 2/26/2024 Last visit: 10/5/2024 Posts: 48 Rating: (0) |
Hello MindFlayer, Would you be able to provide an example on what you are trying to convey? Thanks. |
Follow us on