9/26/2010 11:57 AM | |
Posts: 70 Rating:
|
Hi henk_d If the integrated ethernet card is assigned as a submodule in the PC station then you are able to use T-blocks for socket communication. Create a EC31-RTX project in Step7, use the OC wizard and see for your self. (See my pdf). This will work for all types of WinAC-RTX solutions as long as the Ethernet Card is setup to be IF1 and is supported by WinAC-RTX /soren AttachmentDocument1.pdf (491 Downloads) |
Last edited by: sfa at: 11/4/2010 12:09 PMNo constraints to which IF module is to be used Last edited by: sfa at: 9/26/2010 12:02 PM |
|
10/10/2010 6:27 PM | |
Posts: 947 Rating:
|
EC31 is a widows XP PC-computer. You can write own programmfor communication, such a C++ |
Follow us on