8/23/2019 2:08 PM | |
Joined: 11/12/2012 Last visit: 10/3/2024 Posts: 37 Rating: (3) |
Hello The Audit option is only available for WinCC TIA Advanced/Panels and WinCC V7. From the GMP Manual 6.4 Audit trail The recording of an audit trail for user actions with GMP-relevant data is implemented in the alarm system in WinCC Professional. "Solution" (in the attachment): I will add the comment to the message text and remove the column comment form the alarm view. Regards AttachmentWinCC_Pro_ERES.pdf (179 Downloads) |
Follow us on