12/28/2019 4:36 PM | |
Joined: 12/28/2019 Last visit: 3/2/2022 Posts: 2 Rating: (0) |
Please let us know about EM 235 hardware which is not in step 7 v2.3 software.can i use the above scaling on it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/30/2019 10:25:07New subject after splitting |
|
12/28/2019 6:19 PM | |
Joined: 9/27/2006 Last visit: 5/23/2024 Posts: 12257 Rating: (2668) |
Hello; The EM 235 is an analog input/output module for the S7-200 family. As such it must be programmed with S7-Microwin (now at v4.0 SP9). I believe by v2.3 you are refering to Microwin SMART v2.3, which is for a totally different CPU family. As you can see from the extract below, taken from The S7-200 SMART system manual, there is no EM 235 in the SMART family. You simply cannot use a EM235 module with a S7-200 SMART system. Simply as a curiosity, here is the system manual for the S7-200 CPUs, with all instructions available for Microwin v4.0.: https://support.industry.siemens.com/cs/us/en/view/1109582 The following document will show you the scaling functions for the S7-200 analog modules, and provide you with a downloadable scaling project for Microwin v4.0. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/28/2019 18:20:01Last edited by: dchartier at: 12/28/2019 18:25:29Last edited by: dchartier at: 12/30/2019 11:48:35 |
|