Industry Online Support
Technical Forum
11/5/2015 10:26 AM | |
Posts: 8 Rating: (0) |
u try to modify some settings in file so that it will be out from station than update station and digsi to device |
11/5/2015 10:47 AM | |
Posts: 8 Rating: (0) |
I have tried to upgrade en 100 module firmware upgrade from 4.22 to 4.24 after that in module B firmware it is showing V32.48 AND THE ONLY SOLUTION IS REPLACING MODULE HARDWARE . WHILE NORMALISING IT IS SHOWING AS PER ATTACHED BMP FILE. AttachmentEN100.zip (352 Downloads) |
Last edited by: P Thacker at: 11/5/2015 10:50:22 AM |
|
Follow us on