6/7/2014 1:19 PM | |
Joined: 8/28/2012 Last visit: 9/15/2023 Posts: 39 Rating: (0) |
Please see attachment. Cheers |
6/9/2014 7:55 AM | |
Joined: 9/2/2012 Last visit: 8/15/2024 Posts: 711 Rating: (30) |
Hai, Something strange.. I worked with V11, but not noticed about this property.Now i dont have V11 install also. Better you raisesupport request |
|
|
6/9/2014 9:01 AM | |
Posts: 5225 Rating: (1195) |
You guys are not really comparing apples with apples, are you. Not only is the versions not the same, the license also differs (BASIC vs ADVANCED). And then the KTP600 might even not have that function. I do not have another license other than BASIC, so I can not contribute too much more. BASIC does not have the enable function. We can offerthe invisibility function. Have a picture below to show when the button is not visible. Greetings. w |
This contribution was helpful to1 thankful Users |
5/4/2017 7:39 PM | |
Posts: 2 Rating: (0) |
Hi, It is not the issue with the software or software version. Not all panels support Control Enable. Its a product limitation. Thank you, Sharath Srivatsav |
Follow us on