3/25/2020 8:41 AM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating:
|
Hi, I installed pcs7 v8.2 and did not see the check mark on the faceplate corresponding to the ConPerMon block in the Standard view window 5 (User faceplate 1 button), as shown in the Process Control System PCS 7 APL Operator Guide (V8.2). Is. The description of this button in the document states: I couldn't find a way to display this buuton on faceplate, does anyone know? AttachmentImages.zip (676 Downloads) |
Last edited by: amirab at: 03/25/2020 08:41:40 |
|
3/25/2020 10:35 AM | |
Joined: 9/3/2013 Last visit: 11/3/2023 Posts: 152 Rating:
|
Hello amirab, See APL Manual: https://support.industry.siemens.com/cs/de/en/view/109739941 4.2.8.2 "The visibility of this navigation button depends on the configuration in the engineering system (ES). See also the Opening additional faceplates (Page 191) section for more on this." 1.1.12.2 You can open standard views of other faceplates from various faceplate views. Here, you have the following options: ● Two buttons that you can assign freely and that are used to call faceplates of other blocks. ● Two predefined buttons for calling faceplates with a fixed assignment to the controller blocks. ● Buttons predefined for interlock functions" ff. Regards |
Last edited by: Technodrome at: 03/25/2020 10:36:17Last edited by: Technodrome at: 03/25/2020 10:36:43 |
|
3/25/2020 2:52 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating:
|
Hi Technodrome As shown in the attached image, the CPI parameter of the ConPerMon block was connected to the CPI-In parameter of the PIDConL block but was not seen in the user faceplate 1 snapshot. Best regard AttachmentImages.zip (77 Downloads) |
3/25/2020 6:44 PM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Hi, are you using OS simulation? Then it's known jump to faceplate does not work properly... can't remember the details though |
If I could help you, you can use the RATE button. Thank you. |
|
3/26/2020 11:06 AM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating:
|
Hi Heisenberg2 As shown in the attached image, the CPI parameter of the ConPerMon block was connected to the CPI-In parameter of the PIDConL block but was not seen in the user faceplate 1 snapshot. Best regard AttachmentImages.zip (79 Downloads) |
3/26/2020 2:31 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating:
|
Hi Heisenberg2, As pictures attached, CPI and SelFp1 parameters of ConPerMon interconnected to CPI_In and MV parameters of PIDConL respectively. But User Faceplate 1 is not seen in the ConPerMon faceplate and Control perform in the PIDConL faceplate too as pictures attached. AttachmentImages.zip (81 Downloads) |
3/26/2020 3:30 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi amirab, I have no idea why that doesn't work for you. I have made the connection PIDConL.MV -> ConPerMon.SelFp1 and ConPerMon.CPI -> PIDConL.CPI_In. And now I have at both Faceplate the buttons to jump to the other faceplate (see the attached picture). In your case I would created a Support Request. With regards |
Follow us on