Industry Online Support
Technical Forum
7/12/2012 8:17 AM | |
Posts: 36 Rating:
|
I dont get it... What is the encoder order number? You posted the same encoder as I, and said that its the wrong one...
|
7/16/2012 5:31 PM | |
Posts: 767 Rating:
|
Hello Ententa, It appears you are attempting to identify the part numebr for a replacement encoder for 1PH7184... motor. For this to be identified you will need to provide more information including entire part number and serial number of the motor. The replacement part number depends up on the entire part number (specifically the ninth digit)and date of manufacture according to the design of the motor. Attached is an example name plate for which you may contact below for specific feedback. In the attachment the item labeled "1" is the entire part number which will be 16 digits in length. Item "9" is the serial number. If you are not in North America the below contacts can direct you to your more local support representatives. Customer Support in North America:Phone Hotline: (800) 879-8079 and press "1" Fax: (847) 640-0227 Email: CNCparts.industry@siemens.com Attachment1PH7 Nameplate Example.pdf (415 Downloads) |
7/17/2012 11:37 AM | |
Posts: 36 Rating:
|
Oh... I thought there was one type... Anyway what you mean is probably this:1PH7-184-2ND03-0BC02. |
7/17/2012 10:48 PM | |
Posts: 36 Rating:
|
Heh, just noticed... I actually copy-pasted it from documentation provided by manufacturer. Ill get back to you tommorow |
Follow us on