12/7/2020 2:25 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Use example in attachment to detect only switch point. In the trheshold trigger you can select the gate time e.g. 1s and the amount of pulses in this time to switch anything. Depending on the freqnuecy you need fast counter inputs I3-I6, but not every Logo controller has them. Tell us the order number of your controller to check it. Regards, Scorp AttachmentEncoderSwitch.zip (327 Downloads) |
This contribution was helpful to1 thankful Users |
12/11/2020 6:33 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
If you need an on-signal, just change ON and OFF values of the threshold trigger, see example in attachment. Sometimes it may also a good idea to read the online help of the blocks. Regards, Scorp AttachmentEncoderSwitch2.zip (346 Downloads) |
12/15/2020 10:58 AM | |
Joined: 12/1/2020 Last visit: 8/14/2023 Posts: 19 Rating: (0) |
Hi Scorp I've drawn out what I have , hopefully this will make sense ? Thanks in advance Adam AttachmentLogo Drawing.pdf (325 Downloads) |
Follow us on