Industry Online Support
Technical Forum
1/16/2009 4:58 PM | |
Joined: 9/27/2006 Last visit: 6/3/2024 Posts: 12259 Rating: (2670)
|
Hello plchelp; If you go to the Product Support link at the top of this page, and Search for EnDat 2.2, you will find some FAQs and manuals related to drive systems from Siemens that can use the new absolute encoder format. For example: http://support.automation.siemens.com/WW/view/en/22731584 However, only CNC machines (840D), servos (Simodrive 611) and AC drives (Sinamics, Masterdrive technology board T400) are indicated as useable interfaces, and with some restrictions. There does not seem to be an available interface to the S7-300 PLC family. Hope this helps, Daniel Chartier |
12/2/2010 9:22 PM | |
Posts: 1 Rating: (0) |
Has there been any update to this in the past year. I'm at the same point of wanting to use a EnDat 2.2 with a S7-300. Can this be done. |
12/3/2010 9:46 AM | |
Joined: 4/24/2008 Last visit: 5/16/2024 Posts: 209 Rating: (16) |
There is no update. Only the above named moduls can work with such an encoder. |
|
|
12/15/2010 3:38 PM | |
Joined: 8/27/2009 Last visit: 2/27/2024 Posts: 6 Rating: (0) |
Haidenhain DP Koppler Modul SNr.:18 101 560 B (F6) |
Follow us on