Industry Online Support
Technical Forum
10/7/2024 6:53 PM | |
Joined: 5/6/2022 Last visit: 11/14/2024 Posts: 492 Rating: (99) |
Hi SergeyKrukovich, WinCC is currently in what we call "Delviery Release" which means it is generally avaliable to purchase and is supported. I am unable to provide a date on when it will change its state, but I can tell you that they give support of the current version and the previous version. This means that V7.5 SP2 will still receive patches and security fixes. Please see the documentation below for the details of our product lifecycles. Please see the document below which shows where V7.5 SP2 is within this lifecycle system. Select one product to see the details: Hope this information can help you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on