1/19/2016 3:42 PM | |
Posts: 21 Rating: (3) |
Hi guys, Attached I'm sending the simulation of my loop, now I know that the problem is not "endless loop" but the indirect address of a DB inside the loop. So guys, can anyone help me to identify why at Network 10 (FC53) it is being processed even condition at OB1 not true to call FC53? Because of this I'm getting Event ID 16#2522, the variable used for the indirect addressing is to small when the loop at Network 3 starts. I'm tray to solve the problem, but if anyone can help me I'll very grateful. Thanks a lot. Br, Marciel Fernandes AttachmentPoint of Failure Simulation.rar (178 Downloads) |
1/20/2016 5:43 PM | |
Posts: 21 Rating: (3) |
Hi Piotr.Mr, thanks to answer. The problem related to the OB1 block was solved, but I implemented the solution for FC53/NW3 and the problem keeps happening "Area length error when reading", the variable used to indirect addressing remains large (+). If you can, please verify the attached simulation with solution that you said. Thank you so much ! Br., Marciel Fernandes AttachmentPoint of Failure Simulation 2.rar (182 Downloads) |
Follow us on