1/8/2022 8:13 AM | |
Posts: 3 Rating:
|
Hello Ok, thank you for your answer. The frequency is max 40 Hz, so its low speed. Can i do somewith with a timer? |
1/8/2022 8:19 AM | |
Joined: 12/18/2014 Last visit: 7/11/2024 Posts: 33328 Rating:
|
40 Hz, then must it be possible. Overlap the signals? Are you a encoder? Give more details. |
1/19/2022 4:41 PM | |
Posts: 1 Rating:
|
Hi I send this small program in logo, For higt frecuencies not more than 5 khz supose have to work. Inputs I4 and I5 in a Logo24CE (Fast inputs) And in tge outputs have the sense wich signal came first, I used in small encoders where have 2 signals A and B and low frecuencies but if you are looking for logo for something like this can works. ADPC328
AttachmentDet Cuad A-B.zip (333 Downloads) |
3/11/2022 7:06 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by JOHNAK is split to a separate thread with the subject Would like to activate one output for clockwise rotation and another for counterclockwise rotation. Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to
1 thankful Users |
Follow us on