Industry Online Support
Technical Forum
12/11/2013 2:58 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
run? What exactly is your question? Are you speaking from MODBUS RTU or MODBUS TCP? Do you want to work with the S7-300/S7-400 or S7-1200 or S7-1500? E.g. you can use the CPU 315-2PN/DP with a CP340/ CP341(and the according Modbus RTU license). Here in chapter 6 are some words about more drives with Modbus RTU (S7-1200). |
Best Regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on