11/17/2008 10:11 AM | |
Joined: 5/28/2008 Last visit: 10/7/2024 Posts: 4515 Rating: (839) |
Dear Manju, Actually there are two ways of thinking for your problem. 1. You can easily down load the chart from the internet and think if you can build a polynomial equation for calculation of Enthalpy. I know it won't be easy! 2. If you can reach to a tabels for the enthalpy from the internet or you can make these tabels from the charts.Then, put these values in data blocks; let's say you will have many data blocks and each data block are for certain pressure; and so on. I have a free software for calculating enthalpy. you can download it free from the internet: http://www.et.web.mek.dtu.dk/Coolpack/Files/RefUtil.exe Regards. |
Ayman Elotaify |
|
11/17/2008 5:12 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176) |
Check here www.oscat.lib Free with Sorcecode. |
Karl |
|
11/18/2008 6:34 AM | |
Posts: 39 Rating: (0) |
Hi Karl, I checked out this link www.oscat.lib but it doesn't work. Is there anything wrong with the link? Regards, Manju |
11/18/2008 8:07 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176) |
Sorry, i mean www.oscat.de Here are FCs for Calculate - "Water_density" -"Water_enthalpy" - "Air_density" - "Air_enthalpy" In the Source you can read Information in English. If give a Farum for the OSCAT-LIB to. |
Karl |
|
5/28/2023 10:37 AM | |
Joined: 12/26/2022 Last visit: 5/28/2023 Posts: 2 Rating: (0) |
You need to write the IF-97 Equation into PLC using SCL language. |
6/12/2023 10:02 AM | |
Joined: 3/14/2022 Last visit: 8/30/2024 Posts: 1 Rating: (0) |
Where to find this FB steam? |
Follow us on