1/19/2016 8:57 AM | |
Joined: 10/11/2006 Last visit: 9/30/2024 Posts: 5909 Rating: (806)
|
Hello,
in the following document, there are different examples. https://support.industry.siemens.com/cs/de/en/view/94003334 For linear axis I prefer µm resolution. So you define your gear ratio and your movement on load side. For example if your gear output make´s one turn and your mechanic moves with 200mm, you have 200000LU load side (=200000µm). But with some encoders, you can not reach a µm resolution. So you can choose a resolution of 0,1mm too - so in that case = 200mm = 2000LU.
With "LU" you are absolutely free - so you can define arbitrary units. |
With best regards, |
|
1/20/2016 9:45 AM | |
Posts: 153 Rating: (7) |
Thank you |
2/27/2018 10:38 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
User need to save parameters permantly in ROM. Please refer attached sheet for detail procedure. |
Follow us on