6/20/2024 11:56 AM | |
Joined: 7/19/2022 Last visit: 10/11/2024 Posts: 400 Rating: (63) |
Hello blyshchak, This error usually appears if the IPE file has been created with a version higher than the TIA Portal that you are using to insert the device proxy: Updating a device proxy via an IPE file As indicated, it must be the same version or lower version |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on