12/20/2016 7:39 PM | |
Joined: 12/20/2016 Last visit: 10/3/2024 Posts: 24 Rating: (2) |
While opening the project. Ask for hw-update!! Any help appreciated. Thanks |
12/20/2016 8:09 PM | |
Joined: 3/28/2015 Last visit: 10/4/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following FAQ might help: What is the meaning of the error codes (xxxx:yyyy) in STEP 7? Error number:257:9 The project contains objects of the optional package 'xxxx' that cannot be processed because the optional package is not installed or an outdated version is installed. Cause: The project probably contains objects for which you need an options package that is not installed to process them, or a newer version of the options package. Remedy: Please install the options package concerned. |
Eng.Mohamed Ibrahim |
|
Follow us on