1/31/2012 8:24 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Hello, All of the sudden error 310:3 pops up. I installed SP3 over SP1, no problems. During installation I adapted the security settings. A few days later, I recieved this error. I didn't change anything in the user account or somewhere else...i'm positive. I saw that my login name is in the RC_Maintenance group. I changed to Simatic HMI and after it didn;t work, changed to SQLSERVER2005MSSQLUSER....Also didn't work. I can try reinstalling SQL but I don't know if I can just install again from the cd, or I need to install pcs7 all over again or get a cllean installation. I tried restoring my computer, but it didn't help either. Retrieving an earlier project didn't help either, and I have only one station. Problem is not project related Edit: Station Configuration Editor is giving me an "error" of the type: Proxy saying: Not all applications have logged off from the proxy with index 2. The Siemens helpfile, as always is very helpful: Meaning: Not all applications have logged off in the Proxy function unit with this index Looks that the problem is related to this message. Don't know what it means EDIT2: Automatic updates are off |
Last edited by: Oreca at: 1/31/2012 8:44 AMLast edited by: Oreca at: 1/31/2012 8:32 AMIf I could help you, you can use the RATE button. Thank you. |
|
1/31/2012 10:30 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Update: In Component Services, during my last few minutes on the computer yesterday, an event was called: Source: Userenv User: NT Authority\System Windows saved user domain\es01 registry while an application or service was still using the registry during log off. The memory used by the user's registry has not been freed. The registry will be unloaded when its no longer in use. This is often caused by services running as a user account, try configuring the services to run in either LocalService or NetworkService account. Any ideas?? |
If I could help you, you can use the RATE button. Thank you. |
|
5/21/2012 12:14 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Well, I solved the problem, except I don't now why... Apparantly, my internet connection was lost during start-up. As soon as I was connected again,the project opened without any problems... Maybe there is something in my configuration that causes this? I don't think I need a internet connection just to work with wincc. Can somebodygive me some pointers?? Thx |
If I could help you, you can use the RATE button. Thank you. |
|
5/22/2012 8:23 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Haai, In station configurator: Index 1: IE general which is connected to the plant bus (communication to plc) and usesISO protocol Index 2: Wincc application I have another network card which is normally connected to the internet (terminal bus) and uses TCP/IP protocol. When there is no connection to the internet, the error occurs... Plantbus: Configured mode Terminalbus: PG operation TCP/IP on auto |
Last edited by: Oreca at: 5/22/2012 8:24 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on