1/16/2024 3:52 PM | |
Joined: 7/9/2021 Last visit: 7/21/2024 Posts: 3 Rating:
|
Hello everyone , im using a IM153 as Decentral Peripherie, it uses profibus and it is a slave with the adress N° 2 everytime there is a problem with the comunication between the Master PLC and the IM153, it appers the error #38C4 and the error #39C4, I download the buffer of the PLC, i will copy the buffer down ________________________________________________________________________________ [snip] __________________________________________________________________________ Its Looks like there is a cyclic connection and desconection all the time. Please somebody helpme AttachmentDiagnostic_Buffer.txt (224 Downloads) |
Last edited by: Jen_Moderator at: 01/18/2024 06:04:18Diagnostic buffer added as .txt file. |
|
Follow us on